Vyberte si svoje miesto:

Miesto

KUKA AMP - The automation management platform for Physical AI in industry

KUKA AMP (Automation Management Platform) is an open and modular automation platform that integrates robotics, AI, software, data, and digital services into a centralized environment. It serves as the essential foundation for Physical AI and higher levels of automation.


An intelligent platform for end-to-end automation

AI-powered systems enable greater flexibility and the shift from hard-coded processes to goals formulated in natural language (intent-based automation). In the long term, this paves the way for the autonomous factory. At the same time, many companies must manage increasingly complex and fragmented automation landscapes, with components running in separate systems.

KUKA AMP creates a common data and control layer for the entire automation system and provides a centralized view of all relevant systems and processes. This allows robots, AMRs, machines, software, AI, and data to be connected, coordinated, and continuously optimized across system boundaries. The result is a scalable foundation for the introduction of Physical AI—without having to abandon existing investments.

KUKA AMP at a glance:

  • Combines robotics, software, data, and AI on a single platform

  • Centrally orchestrates robots, AMRs, and automation systems in a vendor-neutral manner

  • Supports planning, simulation, commissioning, and operation throughout the entire lifecycle

  • Enables higher levels of automation through AI and intent-based automation

Ready for the next generation of automation?

Learn how KUKA AMP simplifies automation, connects existing systems, and paves the way for intelligent automation.

Výhody


Leverage Existing Investments

  • Existing systems remain an integral part of the automation solution
  • No costly new investments required
  • Lower integration effort

More Flexible Production

  • Faster adaptation to new products and variants
  • Shorter changeover times
  • Greater agility in responding to fluctuating demand
  • Faster commissioning and shorter project timelines

Introduce AI Step by Step

  • Existing processes remain unchanged
  • New AI capabilities can be added gradually
  • Reduced risk when introducing new technologies

Unified Data Foundation

  • Brings together previously disconnected data sources
  • Greater transparency across processes and equipment
  • A stronger foundation for efficiency, optimization, and AI

Open Ecosystem

  • Supports a wide range of manufacturers and systems
  • No dependency on a single technology provider
  • Future-proof platform strategy

Decades of Industrial Experience

  • Experience gained from more than 550,000 robots installed worldwide
  • Hardware, software, and automation expertise from a single source
  • Practical know-how based on thousands of successfully implemented industrial projects

Successfully Deployed at KTPO

At KTPO, KUKA AMP has become part of regular operations: At the Stellantis production facility, the platforms autonomous mobile robots that execute intralogistics missions at scale. The practical deployment clearly demonstrates the efficiency gains achieved. Among other benefits, commissioning times have been reduced from several weeks to less than 10 minutes.

As a result, new automation solutions can be brought into productive operation much faster, significantly reducing time-to-production.

The KTPO facility demonstrates how existing industrial automation can be strategically enhanced and made more efficient through the combination of robotics, data, and AI.

How does the KUKA AMP automation platform work?

Information from robots, autonomous mobile robots (AMRs), machines, and IT systems is consolidated and used for the AI-powered planning, orchestration, deployment, and optimization of processes.

This enables robots to perceive their environment, evaluate different options, and autonomously decide how to accomplish a task. Instead of programming every step in advance, they increasingly act based on goals and desired outcomes expressed in natural language (Intent-Based Automation).

In this way, Physical AI becomes applicable in real-world production and logistics environments, enabling organizations to gradually achieve higher levels of automation. 

  • Intent and Ecosystem (Business Applications, Open Partner Ecosystem, KUKA Group Competencies)

    KUKA AMP integrates the entire KUKA group competencies of robotics, software, and services—as well as solutions and input from the open partner ecosystem, such as vision technology, and data from business applications like enterprise resource planning (ERP) or warehouse management systems (WMS). This makes KUKA AMP the central platform that brings together the technological infrastructure for automation in one place. 

  • Connect heterogeneous assets

    KUKA AMP brings together applications, data, and hardware from a wide variety of providers—ranging from business software to robots and machines on the shop floor. All operational data from robots, machines, and IT systems is consolidated in a single central location. This creates the integrated data foundation on which all other functions are built.

  • Translate intent into action

    KUKA AMP creates a common language for tasks and environments across all connected technologies. This means that “grasp” or “Station 1” has the same meaning for every system. As a result, AI can understand and process information across systems. Goals formulated in natural language can thus be implemented across different manufacturers without having to program each system individually. 

  • Orchestrate physical operations

    The entire automation process can be planned and orchestrated within KUKA AMP. Various tools are available for this purpose, including a no-code workflow builder that translates natural language commands into executable workflows. This allows complex processes to be created without any programming effort.

  • Operate with visibility

    KUKA AMP serves as the operating system for the entire automation system: Rules and events trigger actions based on predefined rules, while ongoing operations can be monitored in real time at any time—for example, in Live Fleet View. This allows errors and outages to be detected and resolved more quickly, thereby increasing system availability.
  • Optimize continously

    KUKA AMP collects operational data from robots, machines, and other automation systems into a single database. Based on this data, the AI learns from ongoing processes and continuously optimizes them. The digital twin plays a key role: Each process can first be simulated virtually and optimized through multiple simulation cycles involving both AI and humans before it is put into actual operation.
  • Scale with confidence

    Existing automation remains in place and can be expanded step by step to include new systems, applications, and AI capabilities. Companies decide for themselves where traditional automation continues to make sense and where intent-based automation creates additional value.
  • Physical Execution (AMR Fleets, Industrial Robot Fleets, Mobile Manipulation & Humanoid Robots, PLCs & Process Technologies)

    The entire physical execution layer can be centrally managed and orchestrated via KUKA AMP—integrated step by step: robots, conveyor systems, process technologies, and other components from a wide variety of manufacturers. Data from shop-floor operations flows back into KUKA AMP, where it is monitored, analyzed, and used for continuous optimization via AI—thus closing the control loop of execution, monitoring, and optimization.