Puntlassen

Spot welding

Spot welding is a type of resistance welding. The welding process is used primarily in the automotive industry. Using the Delta Spot process, we can even join raw materials, such as aluminum, that cannot be welded normally. 

Spot welding: the technology

Spot welding creates strong joints by means of high pressure in a relatively small area and high energy in the form of electric current. The most important parameters for spot welding are:

  • Current
  • Resistance
  • Heat
  • Pressure

During spot welding, the two welding electrodes press the components together. The weld current is then switched on. The contact resistance results in thermo-electrical heating and the material melts.

The current is then switched off. The molten material hardens, forming a joint that cannot be separated. The pressure must be maintained while the melt is cooling to avoid pore formation.

Automated resistance spot welding with RoboSpin process: shorter cycle times and higher welding quality even for joining aluminium

The robot rotates the servo gun during the welding process, thus significantly increasing the service life of the electrode caps.

KUKA technologies for spot welding applications:

The robots and technology packages from KUKA not only increase the performance of your spot welding applications, they also simplify and minimize their configuration, commissioning, maintenance and service. All this significantly reduces their production costs per part.

Setări module cookie OK și descoperire KUKA

Această pagină web folosește module cookie (mai multe informații) pentru a vă putea oferi cele mai bune servicii și în mediul online. Dacă utilizați în continuare pagina noastră web, utilizăm numai module cookie necesare din punct de vedere tehnic. Dacă faceți clic pe „OK și descoperire KUKA”, sunteți de acord cu utilizarea modulelor cookie pentru marketing. Prin clic pe „Setări module cookie” puteți selecta modulele cookie pe care le utilizăm.

Setări module cookie