Scegli la tua località:

Posizione

Selezionare una lingua:

  • Francese / French
  • Italiano / Italian
Sustainable industrial production

Flexible, Fast and Modular. KUKA Robotics in Caracol’s Additive Manufacturing Platforms

What happens when robotic precision meets additive freedom? Caracol’s platforms, powered by KUKA multi-axis robots, enable scalable, sustainable production of large industrial parts. Operating across sectors such as automotive, aerospace, marine, and architecture, Caracol enables manufacturers to rethink how parts are designed, prototyped, and produced.


Scalable 3D printing with robotics | Caracol and KUKA

Rethink Large-Scale Manufacturing

Founded in 2017 in Barlassina (Italy) and Austin (Texas), Caracol was born from a clear market gap: producing large-scale industrial parts was slow, costly, and highly manual. 
“We started from the idea that producing large-scale parts was too complex, it took too much time, and sometimes it was very, very inefficient for several industrial companies,” explains Francesco De Stefano, Co-founder and CEO.

After two years of R&D, the team launched a platform that merges additive manufacturing with robotics — overcoming the size and flexibility limits of conventional 3D printing. 

 

Where Robotic Additive Manufacturing Outperforms Traditional Methods

Caracol’s large-format additive manufacturing platforms are designed to meet the needs of industries where size, complexity, and performance matter. 
Compared to traditional manufacturing methods, robotic 3D printing offers a fully automated, flexible workflow that reduces waste, speeds up production, and enables on-demand manufacturing. 
“Our customers face inefficiencies in producing large parts,” says Francesco De Stefano. “We offer a scalable, sustainable solution to rethink how and where they manufacture.” 

 

 

KUKA Caracol 3D printing
Automated manufacturing workflows

Turnkey Additive Manufacturing

Caracol delivers fully integrated solutions that combine technology, services, and support tailored to each customer.
“We understood from the beginning that scaling large-format manufacturing isn’t easy,” says Francesco De Stefano. “That’s why we built a platform that combines hardware, software, and automation.”

“We follow the customer through every step,” adds Francesco Sortino, Head of Production. “We help them develop the application, adapt the materials, and deliver a complete solution that enables them to grow their business.”

Caracol 3dprinting lfam rpetg retail design luxury
Caracol Turnkey Additive Manufacturing
KR FORTEC Robot for handling, welding, gluing

Informati sui vantaggi di KR FORTEC

Scopri di più

How Caracol Embeds Circularity into Large-Format Additive Manufacturing

Sustainability is a core principle. Every element is designed to reduce waste, energy use, and environmental impact.

Large-format additive manufacturing minimizes excess by depositing only what’s needed, enabling on-demand production and eliminating molds or inventory.

“Sustainability is at the heart of our business,” says Francesco Sortino. “We don’t just focus on how parts are made, but also on what happens after. Once a component has served its purpose, we can recycle it, re-pelletize it, and use it again — closing the loop.”

Caracol Unique Furniture Design
Caracol unique furniture design

Caracol’s Robotic Platforms for Large-Format 3D Printing

Caracol’s technological core is built around two proprietary platforms: Heron AM and Vipra AM. 
Both systems combine robotics, automation, and advanced software to enable the production of large, complex parts — but each is tailored to different materials and industrial needs.
 
thermoplastic composite printing
3D Printing solutions

Heron AM: Scalable Polymer Printing with Maximum Flexibility

Heron AM is Caracol’s turnkey solution for large-format additive manufacturing with thermoplastics and composites. At its heart is a KUKA KR QUANTEC robotic arm, selected for its precision, payload, and multi-axis flexibility — essential for printing complex geometries up to 10 meters. Its modular architecture includes four extruders — HA (High Accuracy), HV (High Versatility), HF (High Flow) and xHF (extra High Flow)  — allowing it to adapt to a wide range of applications.

“We designed Heron AM to be fast, flexible, and sustainable,” explains Francesco Sortino. “Starting from pellets means lower material costs and faster production, while the robotic system gives us the freedom to print complex geometries at scale.”

KUKA Robotics in Caracol’s Additive Manufacturing Platforms
Caracol Heron AM

Vipra AM: High-Performance Metal Additive Manufacturing

Vipra AM is Caracol’s platform for metal additive manufacturing, based on Wire and Arc Additive Manufacturing (WAAM) technology. It integrates KUKA KR FORTEC robots, selected for their reach, stability, and precision in high-temperature metal deposition.
The system includes two processes: Vipra XQ for high-quality finishing using stainless steels and titanium alloys, and Vipra XP for productivity with aluminum and nickel-based materials.
Caracol Vipra AM
Caracol Vipra AM

Vipra AM is already in use in sectors like aerospace, marine, and composites — for example, in the production of satellite fuel tanks, marine propellers, and tooling for carbon fiber lamination.

Its ability to reduce material waste by up to 90% and enable decentralized production makes it a powerful tool for companies seeking to optimize both performance and sustainability.

“Both platforms, Heron an Vipra share the same DNA,” says Gianrocco Marinelli, Metal Additive Manufacturing Director. “They’re built on robotics, automation, and a deep understanding of industrial applications — that’s what makes them truly scalable.”

Robotics as the Enabler of Scalable Additive Manufacturing

When Caracol set out to rethink how large industrial components could be manufactured, the team quickly realized that additive manufacturing alone wouldn’t be enough.

The ambition was clear: to produce complex, large-scale parts with greater speed, flexibility, and sustainability.

That’s where robotics came in. Caracol integrated multi-axis robotic arms — including KUKA KR QUANTEC and KR FORTEC — for their precision, modularity, and adaptability.

“We understood from the beginning that we needed a support that would allow us to scale the production and make it flexible and modular,” explains Francesco De Stefano. “Robotic arms gave us that flexibility — they’re widely available, cost-effective, and adaptable to the industries we serve.”

This flexibility wasn’t just about movement. It was about integration. Caracol’s approach to large-format additive manufacturing involves combining multiple processes — from material deposition to quality control — into a single, automated workflow.

“Robots are essential because we can leverage multi-axis deposition to manufacture complex geometries,” adds Gianrocco Marinelli. “We’re not limited to planar slicing — we can work in cylindrical coordinates, which opens up entirely new possibilities for design and production.”

Beyond the hardware, software plays a critical role. Caracol’s platforms leverage first its proprietary software suite, Eidos Manufacturing: with its slicing module and IoT for process control. Furthermore, for Vipra also the use of advanced packages like Architect and Robot Sensor Interface to monitor and control the deposition process in real time. These tools allow the system to adjust parameters dynamically, ensuring consistent quality even in the most demanding applications.

Scalable robotic 3D printing for large parts
[Scalable Robotic for 3D Printing]

A Strategic Partnership for Scalable Robotics Integration

“We decided to partner with KUKA because the technology offered the right trade-off between accuracy, cost, and reliability,” explains Francesco De Stefano. “It also allowed us to integrate our software and hardware more deeply into a turnkey platform.”

KUKA’s modular architecture — including expandable rails and rotary tables — gave Caracol the flexibility to adapt to complex geometries without compromising efficiency.

KUKA Caracol partnership

“This flexibility allows us to create custom applications tailored to our clients' requirements,” adds Francesco Sortino. Beyond integration, KUKA’s global customer service network played a key role in supporting Caracol’s international growth. “We needed a global partner that could help us scale at the speed we were growing,” says Francesco De Stefano. “KUKA’s infrastructure enabled us to support customers worldwide and ensure inventory availability through framework agreements.”

Beyond technical integration, the partnership also supported Caracol’s global expansion. With customers in over 50 countries and operations spanning Italy, the US, and the Middle East, having a robotics provider with international infrastructure was crucial.

Building Tomorrow Factory

Caracol’s vision goes beyond 3D printing: it’s about full automation. “Our true vision is to enable different fleets of robots producing on demand in different areas of the continent,” says Francesco De Stefano.

To make this happen, Caracol is piloting autonomous mobile robots (AMRs) to automate internal logistics.

While Heron and Vipra AM handle manufacturing, AMRs take care of what happens around it — moving parts across the facility without human intervention. “We’re working on how to automate the factory floor — not just for us, but for our customers as well,” Francesco De Stefano explains.

AMRs integrate seamlessly into Caracol’s digital workflow, connecting production and logistics in real time.

Combined with KUKA’s global customer service and automation expertise, this approach helps Caracol deliver scalable, autonomous solutions that go far beyond the printhead.

AMR 3d printing
AMRs by KUKA for Caracol Application

KUKA’s infrastructure enabled us to support customers worldwide and ensure inventory availability through framework agreements.

Francesco De Stefano, Co-founder and CEO - Caracol

Trova i KUKA System Partner vicini a te

Qui trovi il partner giusto per il tuo settore o il tuo problema.

Potrebbe anche interessarti