In the world of premium hat making, every detail matters. Behind the creation of a hat lies an essential element: the wooden hat block on which the felt is shaped to achieve its final silhouette. This is precisely the craft of L’Autre Instant, a company founded by Mathieu Henra and his business partner Lucille Bac. Specializing in the design and manufacture of wooden hat blocks for the hat-making industry, the company preserves a particularly rare artisanal expertise, now threatened by the gradual disappearance of traditional hat block makers.
In this context, the challenge was clear: to modernize production capabilities while maintaining the quality standards and precision that define this exceptional craft.
A drive to push the boundaries of traditional machining
To manufacture its wooden hat blocks, L’Autre Instant initially relied on conventional 3-axis machining machines. Although this equipment met the company’s needs, it nevertheless limited the geometric complexity of the parts that could be produced.
A robotic solution tailored to the industry's requirements
To meet this specific need, KUKA and 3IDM (Robotmaster distributor) supported the company in the integration of a 5-axis industrial robot dedicated to machining operations. Beyond the robot itself, the project also relies on 3IDM’s software expertise, enabling the company to fully leverage the capabilities of the installation.
This new solution enables:
• the machining of far more complex shapes;
• the maintenance of an exceptionally high level of precision;
• greater design flexibility;
• the modernization of a traditional craft without altering its essence.
The power of digital technology serving craftsmanship
The integration of software solutions developed and distributed by 3IDM, such as Robotmaster, plays a key role in the success of the project. Thanks to advanced 3D modeling and simulation tools, machining programs can be validated beforehand, significantly reducing testing and setup times and enabling a satisfactory result to be achieved on the first attempt, without the need for physical testing.
The cornerstone of this project lies in the ability to leverage data from the software environment already used by the customer. This approach made it possible to simplify integration, minimize the need for custom development, and significantly reduce the costs associated with the project.
Comprehensive support from design to commissioning
The success of the project also relies on the complementary expertise of KUKA’s teams, responsible for robotics expertise, and those of 3IDM, specialists in software, simulation, and technical support.
Thanks to this support, L’Autre Instant was able to carry out a large part of the integration independently, while benefiting from the assistance needed to quickly unlock the full potential of its new installation.
This collaboration demonstrates that even a niche artisanal business can now access advanced robotic technologies and integrate them effectively into its operations.
A concrete example of innovation supporting the preservation and transmission of craftsmanship
In a profession where the transmission of expertise is becoming increasingly challenging, automation does not replace the craftsperson. On the contrary, it provides new ways to express and enhance their expertise.
By combining the flexibility of a KUKA industrial robot, the digital tools of 3IDM, and the unique know-how of L’Autre Instant, this project demonstrates that tradition and innovation can move forward together, coexisting to ensure the long-term sustainability of a rare craft and prepare it for the future.