Humanoid Robots in Manufacturing
Humanoid robots are robotic systems with human-like characteristics that can perform complex tasks. KUKA is pursuing the use of humanoid robots with a focus on autonomous systems that create concrete added value in real production environments. How far has the development of such systems progressed? And in which areas are humanoid robots used today? In this article, we take a look behind the technology and show how humanoid robots are shaping the future of manufacturing.
Do humanoid robots already exist?
KUKA does not see humanoid robotics as a short-term product goal, but as part of a broader vision. Everything is framed within the concept of “Physical AI” – the interplay between hard-ware and software, and our Automation Management Platform – a single pane of glass for our robot fleets.
Who builds humanoid robots?
KUKA is pursuing the use of humanoid robots with a focus on autonomous systems based on mobile platforms and equipped with AI, sensor technology, and gripping technology.
Our focus is on autonomous mobile manipulation robotics (AMMR), physical AI autonomous systems, as well as digital twins and simulation. By combining mobile platforms, robotic arms, and AI, we focus on industrial and professional logistic service markets.
Where are humanoid robots used?
Currently, the focus is on simple handling tasks in logistics, among other things. In the future, humanoid robots could also be used for more complex tasks in assembly, maintenance, or service—anywhere where flexibility and autonomous decision-making are required.
The frequently cited advantages of humanoid systems – mobility, ambidexterity, and high flexibility – are key requirements for customers in industry. KUKA therefore focuses on the following aspects, which are crucial for autonomous robot systems:
- Mobile platforms with high flexibility
- Sensors and vision systems, especially AI-supported image processing
- Variable gripper systems for different tasks
- Open interfaces for maximum integration capability
- Simulation for training and optimizing the application
KUKA can thus already cover many possible areas of application for humanoids very efficiently with existing solutions:
- Autonomous mobile robots (AMRs) perform tasks in logistics, production, and even healthcare. They navigate independently, work collaboratively with humans, and can be flexibly integrated into existing processes. Examples such as the smart factory at KRONE or automated furniture production with Formetal show how mobile platforms from KUKA create real added value. With autonomous mobile manipulators, KUKA offers modular, driverless platforms that are combined with robot arms. They are highly flexible, scalable, and ideal for applications such as material transport, order picking, collaborative manufacturing, and healthcare.
- Central real-time control of heterogeneous AMR fleets with AI-supported planning, optimized processes, and simple, programming-free integration into existing systems.
- In addition, KUKA offers iiQWorks.Sim simulation software, a powerful tool for virtual commissioning and offline programming of cobot applications on the KMR iisy platform. This allows customers to simulate, optimize, and validate the respective cobot application in advance while the platform is stationary.
- With Visual Components, the KUKA Group provides a powerful 3D simulation platform on which entire factories can be planned virtually, processes checked, and production flows optimized—even before the actual commissioning takes place.
- With Swisslog, the KUKA Group offers intelligent automation solutions for warehouses and logistics that optimize material flows and make picking processes more efficient.
- Swisslog Healthcare supplies automated systems for hospitals and pharmacies, such as pneumatic tube and medication management solutions, which take over routine tasks and thus relieve staff.
Which industries benefit most from humanoid robotics?
Can I buy a humanoid robot?
What does the future of humanoid robots look like?