請選擇您的所在位置:

國家

LBR IIWA draws selfies of visitors

KUKA robots in the “Kreative Robotik” exhibition at the Ars Electronica Center (AEC) in Linz

2016年2月26日


The LBR iiwa holds a calligraphy pen. KUKA robots create art at the “Kreative Robotik” exhibition. In the foyer of the Austrian Ars Electronica Centers (AEC), the LBR iiwa and the KUKA KR 16 – an industrial robot for low payloads – demonstrate how humans and machines can work creatively together.

KUKA lightweight robot calculates the brightness of pixels 

In the robotics laboratory at the University of Art and Design Linz, the LBR iiwa has learnt a new skill. It is presenting it in the foyer of the AEC. It photographs a visitor and then calculates the brightness of each individual pixel. It then uses the calligraphy pen to reproduce the photo. For this, the lightweight robot uses the narrow side of the nib for every light pixel. For each dark pixel, it uses the broad side. In this way, a clear replica of the photo is gradually produced.


The LBR iiwa uses a calligraphy pen to replicate photos of visitors.

KUKA robot for low payloads draws light motifs

The industrial robot swings an LED wand to create light motifs at the exhibition. This is achieved using long exposure times and corresponding software. The images are displayed on a screen. And also in the Deep Space of the AEC. The developer of the technology is Chris Noelle from the University of Art and Design Linz.
The drawing LBR iiwa and the entire art exhibition at the AEC were a co-production of the University of Art and Design Linz, the Association for Robots in Architecture, the RWTH Aachen University and KUKA Roboter CEE GmbH.
LBR IIWA DRAWS SELFIES OF VISITORS

我們使用 Cookie

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定