KUKA Brings the Future of Cobot Automation to IMTS
Debuting what it terms Sensitive Cobotics, KUKA Robotics will show IMTS attendees the future of automation in the form of its new LBR iisy cobot. As ready-to-use automation, the LBR iisy quickly and easily integrates into any manufacturing application from pre-defined production processes to open, unstructured work environments with unpredictable conditions from one job to the next
August 12, 2022
For show attendees in the automotive, e-mobility, aerospace, electronics and related industries, the company will demonstrate advanced automated friction stir welding (FSW), a process that fulfills the growing need for fast, clean, reliable and cost-effective joining for non-ferrous metals and mixed metal combinations frequently encountered in fabricating such components as electric vehicle (EV) battery housings and trays.
With six axes, a 3-kg payload, 600-mm maximum reach and 18.8-kg overall weight, the LBR iisy is well suited for overcoming the challenges posed by confined workspaces. Whether loading/unloading machines, assembling components or packaging, the cobot provides increased versatility and can be immediately operated by anyone from an automation expert to a cobotics newcomer. Featuring various operator levels, the user-friendly system adapts to the corresponding level of user knowledge.
The LBR iisy is fully embedded into the KUKA Industry 4.0 ecosystem. In addition to the availability of downloadable software apps, the company’s KUKA Connect cloud solution allows users to access and analyze the cobot’s data at any time.
Despite its low procurement costs, the LBR iisy is equipped with high-grade joint torque sensors integrated in all its axes. These sensors respond to the slightest of external forces and provide certified collision protection.
As part of a live demonstration, IMTS attendees will also see KUKA’s robotic FSW process welding aluminum parts to manufacture an assembly. The cell will consist of multiple robots. One robot will pick parts from bins and place them into a fixture and a second robot will perform FSW using both Roboception and SICK PLB 3D vision technologies.
For EV battery tray production, KUKA has engineered its cost-effective KUKA cell4_FSW modules to provide up to 95% more process efficiency and maximize the available configuration options for manufacturers. Used for both 2D and 3D welding tasks, the modules are scalable and accommodate either one or two 6-axis robots. Shops can arrange several workpiece clamping tools in the working area of the cell so that robots can work simultaneously on larger components if needed.