Select your location:

Country

Select your language:

  • German
  • English
  • English
  • German
  • English
  • German
  • English
  • English

Success factors in automation in the electronics industry

Automation transforms productivity in virtually every form of manufacturing, and electronics is no exception. In this article, you’ll learn what’s most important about automation in this industry and how growth in the electronics industry is driving robot innovation.


Guest author
July 20, 2021
Imagine
Reading Time: 2 min.

By Kaile Hodgens

Automation transforms productivity in virtually every form of manufacturing, and electronics is no exception. In this article, you’ll learn what’s most important about automation in this industry and how growth in the electronics industry is driving robot innovation.

In contrast to the large, powerful robots that move chassis in the automotive industry or palletize beverage crates, the electronics industry requires speed and precision when handling small, delicate components:

Factor Speed

Electronics applications demand speedy robots with low cycle times, preferably below 0.4 seconds. The cycles themselves must be tuned to manipulate small items with care.

Factor Precision

Accuracy and repeatability are fundamental to the types of product manipulations involved in electronics manufacturing. Pose repeatability of 0.02 mm is ideal for these tightly structured tasks.

But these are just two factors that play a major role in robot-based automation in the electronics industry. This is because, especially in semiconductor manufacturing, many electronics production lines operate in cleanroom environments and require robotics with the correct cleanliness-class certification to function correctly under these circumstances.

Man and robot in high-purity production environment: highly automated semiconductor factory of the future.

Faktor Umgebung

Many applications in the electronics industry rely on cleanroom environments to protect sensitive products from contamination. Humidity can also play a role here. In addition, the systems usually have to be integrated compactly with optimum use of the available space, oftenwith limited access for service and maintenance. Electronics manufacturing also requires a compact, low-energy controller. To create small working cells, robots need internally routed power and air supply for their attachments. It requires robots with a small installation area and an ultra-compact overall design.

All factors require automation solutions to be specifically geared to the electronics industry. This leads to ever new innovations, because the pulse of the electronics industry is fast. Developments have to be agile and so, for example, mobile robots for semiconductor production or cobots are establishing themselves in electronics manufacturing.
About the author
Next article

We are using Cookies

This website uses cookies (find out more) in order to offer you the best service online as well. If you simply continue to use our website, we will only use cookies required for technical purposes. If you click on “OK and discover KUKA”, you are also agreeing to the additional use of marketing cookies. You can select which cookies we use by clicking on “Cookie settings”.

Cookie settings