Select your location:

Country

Select your language:

  • German
  • English
  • German
  • English
  • German
  • English

From Delta to Scara: Overview of industrial robot types

Hundreds of thousands of robots are in operation around the world every day. Their appearance is as varied as their tasks. Here we present a few of the most important representative types.


ARTICULATED

 

The archetypal robots in industrial manufacturing, articulated robots have rotational main axes and can thus generally move freely in space. The most widespread design has six axes, while a seventh axis basically enables the robot to ‘work around the corner’.

In order to extend the working range still further, it can be mounted on a linear axis, thus covering longer distances or serving multiple work stations. Articulated robots – including dual-arm systems – are primarily used for flexible tasks, particularly ones involving complex motion sequences. The robot can perform a wide range of tasks, such as assembly, palletization, spot welding or painting.

DELTA

The shape of these robots is reminiscent of the Greek letter delta. They are parallel arm robots with tripod kinematics and their arms are connected to universal joints at the base. A key feature of delta robots is that their main drives are fixed on the frame. Moreover, they generally have three or four degrees of freedom. The base of the robot is mounted above the moving parts, i. e. suspended from the ceiling.

The jointed arms – at least three – start here and are connected to a small triangular platform at the other end. Delta robots are fast and light and are thus frequently used for packaging and assembly tasks and in high-speed applications. Thanks to their precision, they are suitable for pick-and-place tasks, while their speed means that they are also suited to very high-volume applications in the pharmaceutical industry.

SCARA

The SCARA robot – short for Selective Compliance Assembly Robot Arm – stands on a stationary base and has a swiveling jointed arm with three vertical rotational axes. SCARA robots are also characterized by the fact that they have fewer than six degrees of freedom – normally four.

At the end is the vertical and rotational Z axis on which a gripper can be mounted. Typical tasks are horizontal transfer and vertical joining. The robust robots can be installed on the floor, wall or ceiling. SCARA robots require little space and have high repeatability. However, they can only be used for low payloads and a small workspace.

GANTRY

Gantry robots can transfer loads over long distances and position them with great precision. Smaller versions of gantry robots also exist in pick-and-place machines. Gantry robots load machines from above, for example via loading hatches – so the machine remains accessible. Different gantry robot variants are available.The simplest variant is the linear gantry.

Here, the points to which the gripper can be moved are located in a single axis. The gantry arm is responsible for the vertical motions while a gantry slide performs the horizontal motions. If a perpendicular motion is also required, a cantilever gantry is used. A Cartesian gantry robot can cover large areas.

PALLETIZING ROBOT

This robot automatically places pallets and packages on load carriers. It comes in various types, such as the layer palletizing robot. Palletizing robots generally have four degrees of freedom. They are very powerful and are used to place entire loads on a pallet. The tool flange of the palletizing robot, and thus also the tool itself, always moves parallel to the floor.
About the author
Teresa Fischer

Spokesperson Business KUKA


More about Teresa Fischer
Next article

This website uses cookies (find out more) in order to offer you the best service online as well. If you simply continue to use our website, we will only use cookies required for technical purposes. If you click on “OK and discover KUKA”, you are also agreeing to the additional use of marketing cookies. You can select which cookies we use by clicking on “Cookie settings”.

Cookie settings