LBR iiwa on tour in Germany
Human-robot collaboration (HRC) is playing an ever greater role in production. There are also other fields of application, however. For a project with Vodafone, an LBR iiwa is luring visitors into Vodafone stores in six cities and drawing selfies
30 June 2016

LBR iiwa – the lightweight robot artist
If the customer wishes to have a portrait drawn by the robot, a Huawei P9 first takes a picture and forwards it to a computer. There, a software package specially developed by KUKA and Vodafone converts the image into a vector graphic. The data are then transferred to the LBR iiwa. Using the vector graphic, the robot starts to draw. The amazing thing is that the robot decides for itself where to place the lines. After about ten minutes, the robot is finished with the drawing and the visitor can take the special souvenir away.The tour dates and venues for the LBR iiwa are as follows:
- 16.06. – 18.06. Munich, Marienplatz 25
- 23.06. – 25.06. Hamburg, Jungfernstieg 14
- 30.06. – 03.07. Dortmund, Westenhellweg 52
- 07.07. – 09.07. Düsseldorf, Flinger Straße 40
- 14.07. – 16.07. Cologne, Schildergasse 69-73
- 21.07. – 23.07. Frankfurt, Zeil 85