Välj din plats:

Land

Video

Team CoNeeBot (Hamburg University of Technology, Germany)

Needles are important instruments for carrying out minimally invasive treatments such as biopsies. There is a long history of investigating image-assisted processes and robotics in order to provide support during precise needle positioning. Up to now, this has mostly involved aligning the needle with the target using the robot. The doctor then has the task of moving the needle into the target area. This task is made more difficult through deformations in soft tissue as well as through a bending of the needle upon insertion. Team CoNeeBot’s goal is to develop a smart needle that recognizes its environment, to connect it to the robot and thus to help doctors in the correct positioning of the needle.