KR CYBERTECH: streamlined robot for high speed and maximum reach
The KR CYBERTECH industrial robot is suitable for machining and handling large components as well as for assembly, palletizing and arc welding. Now, it has also won an accolade for its design. The jury’s reasoning: “The KR CYBERTECH industrial robot – with its streamlined, elongated silhouette – stretches the limits of possibility in terms of speed and reach.”
Economical use of materials reduces energy consumption
With a reach of 2,100 mm, the robot covers extremely large distances for its payload category of 20 kg. This was impossible for predecessor models.The economical use of materials also reduces energy consumption and supports sustainability. “It is designed to be fast and agile, reliable and precise. The robot also has to cover a large workspace and be extremely flexible in terms of deployment so that it is ideally suited for use in many applications in industrial production and can tap into new sectors,” says industrial designer Mario Selic. The robot can be installed on the floor, wall or ceiling, or at a certain angle.
Customers profit from the compactness of the KR CYBERTECH robot
The KR CYBERTECH is the answer to the ever-increasing requirements in automation.
It sets a new benchmark in performance and power density. With its utmost precision and a repeatability of 40 micrometers, it can exploit its strengths to the full – even at maximum speed.Customers profit from the volume-reducing compactness and outstanding freedom in production: the robot masterfully unlocks a workspace of 23 m3 in volume.